Hi,
my Problem is, that i have to use the Command Expert Tool without an internet connection.
Therefore i downloaded the offline Command Expert Package from Keysight.
But when i try to install those as describet in the Manual i get the message attached.
It says:
"Failed to install command set 'InfiniiVision 6000 Series Oscilloscopes'. Der Typ 'Agilent.CommandExpert.ScpiNet.AgInfiniiVision6000_06_10_0001.SCPI.MEASure.VTIMe.VTIMeClass' definiert bereits einen Member namens 'Query' mit den gleichen Parametertypen."
This happens with all Command sets and is not related to this one set.
I've also tried to install the sets, that are on the original CD, that came with the device itself.
But here i had no luck, too.
Further i tried to reinstall the complete tool, unfortunately no luck.
Can someone help me here?
Thank you
This is a question that should be addressed by your local Technical Call Center. Go to www.keysight.com/find/contactus for your local contact information.
The Keysight Forums are not intended as a means to contact Keysight Technical Support. They are only occasionally monitored by Keysight technical personnel.
Al