Hello,
I have ran into a wall after a wall during attempts to downgrade 1683AD back to A.03.67. Turns out our repair vendor upgraded this instrument while servicing it to WinXP Service pack 3 which looking at other articles in this forum have caused incompatibility issues.
My take is to try to restore my LA back to original image and install A.03.67 at that point.
Would it be still possible to upload image 01680-14106 to: ftp://ftp.agilent.com/cos/outbound/16xxx%20recovery%20images/01680-14106?
Thank you.
We moved from the Agilent site almost 4 years ago, and then there were abuses of the Keysight ftp site, so IT mostly shut us down.
The three CD images are here, temporarily. I will delete them in a week or so.
Dropbox - 01680-14106 - Simplify your life
Al