AnsweredAssumed Answered

External Testset Control

Question asked by 68carlsson on Dec 6, 2006
Latest reply on Jan 16, 2007 by daras
Have two question about the Testset control with the PNA which enables switch control before taken a channel sweep.

1. How is the idea to make this possible from remote SCPI/COM?
One workaround is to make the test software create an XML-file and copy this to the PNA hard drive. A drawback using this is that the programmer needs to fully understand the items to specify in XML.

2. What about ethernet controlled switches?
Seems like the future interface to use is either LAN or USB (LXI).
How can I solve testset control of a ethernet controlled switch.  

Outcomes