I will like to simulate the phase noise of a BJT amplifier including flicker noise sources for the Ic and Ib currents, the parameters of theses sources like Kf and Af i have extracted through measurements. I have seen that ADS has a noise current source I_NoiseDB and voltage source V_NoiseDB that can produce flicker noise components.When I try to implement the source of the schematic I dont understand what should I put for the "Element" and "Pin" values and how I can associate them with the base and collector currents of my device. Any help will be apreciated
and how can flicker noise generated to add in dc source?
Suggest using the BJT_Model item, which has parameters for flicker noise. This model is used in conjunction with a BJT device like BJT_NPN, BJT_PNP. etc.