AnsweredAssumed Answered

N8990C-R47 Switch commands

Question asked by reyes136 on Aug 22, 2018

I am using an old N8990C-R47 Switch, currently we are adding it to our network with the following commands.

IP:ADDRESS?

IP:ADDRESS 192.168.1.10

IP:SUBNET:MASK "255.255.255.0"

 

These are the only commands I can find to setup the switch. We also have newer versions of the switch that accepts other commands.

SYST:COMM:LAN:DHCP "0"
SYST:COMM:LAN:GATE " "
SYST:COMM:LAN:IPAD " "
SYST:COMM:LAN:MAC?

 

These commands do not work on the older switch. Does anyone have a list of commands that will work on the older switch? Mainly the command if there is one to put the switch on DHCP.

Outcomes