AnsweredAssumed Answered

Save and recall Calibration settings

Question asked by gabmorod on Nov 10, 2006
Latest reply on Sep 17, 2009 by michelbraga
A simple question that I haven't found in the manuals but I'm sure it must be somewhere.
I want to use an agilent 4395 A to perform S11 measurements. So, I want to perform some calibration set ups and record them into memory so that they can be recalled afterwards by using the GPIB.
How can I save the calibration settings?
How can I recall those calibration settings?

Thanks a lot

P.S: Sorry to include the same question into two topics, but I'm not sure where is the best position for it. Admin, feel free to erase one of them if you find it necessary  

Outcomes