AnsweredAssumed Answered

Synchronizing N5230A and PC when communicating with LAN sock

Question asked by wleippe on Dec 6, 2007
Latest reply on Dec 11, 2007 by dgun
When looking for data back from the PNA I make sure the MAV bit in the status byte register is set by using vireadstb, this works fine under gpib, but when I try to do it using sockets I get an error 0xBFFF003A VI_ERROR_INV_SETUP unable to start operation because setup is invalid. If this is the case how should I synchronize my PC and the PNA so I don't try to read back data to soon.  

Outcomes