AnsweredAssumed Answered

Transfer speed of PNA-data

Question asked by jogo on Nov 12, 2007
Latest reply on Nov 14, 2007 by jogo
Hi,

I use Linux, a LAN-connection and communicate via sockets with the PNA. My program queries data in s2p-format, real/imaginary exposition. If I start a measurement of all four S-parameters, it takes about 20 seconds until data are available on the remote pc, regardless of which amount of sweep points I choose. In my opinion it's a very long time. Has anybody an idea what I can do to accelerate transfer speed? I also noticed that time interval between sending the first command to reset the pna and pna resets is about several seconds... Is it normal?
Thanks for your support!

Regards,
John  

Outcomes