AnsweredAssumed Answered

Synchronize multiple Waveforms with ext Trigger

Question asked by Sergey013 on Aug 7, 2018
Latest reply on Aug 13, 2018 by jonathan.falco

Using two M3201A devices. I facing a problem trying to synchronize multiple AWG by external trigger.

The waveforms are loaded in device's memory and queued. The trigger is configured for external raising edge. Trigger signal is a 100us pulse 0..5V connected to Trigger I/O from external generator.

Tried Labview code and Keysight SD1 SFP software - everything works fine when trigger is disabled, but no output when ext. trigger is configured.

 

Your support as Source-code or LabView diagram is appreciated.

Outcomes