Is there a method of incorporating the a DAQ unit into the Benchvue test sequence such that the data recorded from the DAQ can be exported in a CSV file once being captured? Currently in the test sequence the data exported will only provide whether the DAQ has started, stopped, or swept once. Ideally, the exported data should provide information collected by the DAQ as well as information collected by Benchvue (e.g. the current and voltage measurements).
Is this possible? I know I can export the data from the DAQ separately, but would like to automate the process using the Benchvue test sequence. Thank you.
It's coming soon to a theater near you! Seriously, the next DAQ App release will have the ability to export data by dragging the Export button from the app into Test Flow. There are other enhancements coming to the app too. Should be released in early October.
Brian