AnsweredAssumed Answered

IntuiLink Waveform Editor and IO Libraries Suite can't be installed in the same OS

Question asked by lzhmark on Jul 23, 2018

I want to use IntuiLink Waveform Editor for Function/Arbitrary Waveform Generators to create my own pulse signal over 33250a generator. When I run it, the error said it needs IO Libraries Suite. But the version of IO Libraries Suite I can get is for win 7,8, and 10, not for win XP. At the same time, the IntuiLink Waveform Editor for Function/Arbitrary Waveform Generators only can be run in win XP. So anyone has an idea to solve it. Appreciate it!

Outcomes