AnsweredAssumed Answered

Measuring the time of several pulses

Question asked by flexo on Jul 20, 2018
Latest reply on Jan 16, 2019 by louismarais

We use a older HP 53132A in our company and now we bought a Keysight 53220A as a replacement. Now I want do the following measurement: count a certain number of pulses (e.g. 100) and measure the total duration time until the number is reached. Then reset the duration and count again.

 

With the old HP, this is described very well in the manual on page 2-21:

I just don't get it. The new Keysight has an overwhelming number of options. Do I just not find this or can this counter not?

Outcomes