Hello,
I can easily save waveform using the following command.
I can also select only the Math channel by using the following command:
But I don't know what command I should use to export FFT signal in CSV.
Regards,
Ivan
Dear @hognala, it would be great if you can help!
Hi Ivan,
Saving the FFT waveform should be the same as saving the channel 1 waveform, except you ":DIGitize FUNCtion", set ":WAVeform:SOURce FUNCtion", and use ":WAVeform:POINts:MODE MAXimum" (or NORMal, but not RAW).
Best Regards,
Pat