AnsweredAssumed Answered

E5071B marker display position

Question asked by Warren on Feb 8, 2008
Latest reply on Feb 12, 2008 by RayH
Is there a way to relocate the marker display position on the E5071B network analyzer?  Often the sweep goes through the text and the curve is obscured.  Other than removing the text entirely, can it be relocated to another position on the screen such as the upper or lower right corners as needed?  Another improvement would be changing text size.  Can the marker text font be changed or reduced?  

Outcomes