AnsweredAssumed Answered

Z5623AH50 Multiport Test Set

Question asked by dhamilton on Nov 7, 2011
I have a Z5623A H50 Multiport test set which I believe is the predecessor to the N4221A and the N4421B.   Can I use this with a properly configured E8263B or E8364B?  If so, do I require a software package to use it?   Also, if there is any documentation on it would be great.  

Outcomes