AnsweredAssumed Answered

How to trigger FieldFox when average on with SCPI commands

Question asked by nadia1989 on May 23, 2018
Latest reply on May 26, 2018 by nadia1989

In ENA, when average is turned on, I use command to turn on the average trigger, therefore one "INIT" can let the ENA do several sweeps according to the average counts.

 

In PNA-X, there is no average trigger command on the panel. And I use the group sweep mode to trigger the VNA and let the VNA do several sweeps.

 

BUT in Fieldfox, there is no average trigger and group sweep mode, how should I trigger the VNA with SCPI commands when the average is turned on.

Outcomes