I would like to use the Agilent 34925A MUX module in the 34980A mainframe to run a LabVIEW program that continuously scans 10 2Wire resistors. The problem is that the A BUS (911) relay is repeatedly opened and closed each time it is scanned.
In the Agilent BenchLink Data Logger Pro demo program, A BUS (911) remains ON and the SCANNIG or INTERVAL alternately appear on the 34980A panel and the data is recorded continuously.
As with the Agilent BenchLink Data Logger Pro program, I would like to ask if there is a way to measure 1001 ~ 1010channels continuously while keeping A BUS (911) ON using LabView program.
In the Agilent BenchLink Data Logger Pro demo program, A BUS (911) remains ON and the SCANNIG or INTERVAL alternately appear on the 34980A panel and the data is recorded continuously.
As with the Agilent BenchLink Data Logger Pro program, I would like to ask if there is a way to measure 1001 ~ 1010channels continuously while keeping A BUS (911) ON using LabView program.
I would really appreciate your help.
Thank you.
This should not happen if the LabView driver correctly programmed the 34980A. Are you using the driver from NI or the one from Keysight (formerly Agilent). You can download the Keysight version at https://www.keysight.com/main/software.jspx?ckey=1628832&lc=eng&cc=US&nid=-33260.536894538&id=1628832