Hello all
I am using ADS 2017. And I like to use the sensitivity analysis.
Unfortunately, I couldn't find any document explaining the influence of the properties in the "goal" object over the sensitivity analysis.
I understand that probably Expression is the Y in the sensitivity equation that is finally based on the Analysis simulation like Harmonic Balance.
What is the influence of LIMIT in goal object?
By trial and error, I found out that limiting in frequency influences the sensitivity. But I do not know how exactly is it calculated for a range of frequency? (I am using Harmonic Balance)
What is the influence of limit1, Type, Min. Max, Weight in the sensitivity analysis? Are they somehow included or just ignored?
Best regards
Mamad
I am updating this post since I found some documents "About_Sensitivity_Analysis" in ADS but it is still enough"
"if a goal contains several simulation points, only the point with the highest sensitivity is reported."
I still do not know the function of limit in the goal settings in sensitivity analysis.