AnsweredAssumed Answered

8720 Tuned Receiver Mode

Question asked by brdavis32 on Nov 7, 2010
Latest reply on Nov 8, 2010 by brdavis32
I am struggling to find documentation for operating my 8720ES in tuned receiver mode - this is a new function for me having only used it in S-parameter mode previously. I can enter it into the 'tuned receiver' mode, but the proper configuration of my system to support that is not clear. I have an MXG signal generator and the first step that i wish to accomplish is to simply detect the RF out signal using the 8720ES in tuned receiver mode. I have made the 10 MHz ref connection, but what are the settings and screen to use on the VNA as the reeciver and which parameters do I watch?

thanks for any help.  

Outcomes