AnsweredAssumed Answered

8515A

Question asked by Franz on Jan 5, 2008
Latest reply on Jan 9, 2008 by RayH
Hello,
I intend to buy a used 8515A . Does the item function , if the maybe semi rigid cable on the back are not present ? Which function have this parts ?
I intend to use more than one S-Parameter Testset . Normally Option 001
is needed . Some items have no sign 001 , but two connectors for the appropiate cable . Have every item Option001 , if there are two connectors or have every item these two connectors and the electrical
connection inside is not present , if not 001 ?
Thank you for answer from Franz .  

Outcomes