AnsweredAssumed Answered

Golden-Mixer Technique

Question asked by lalalu on Jul 4, 2010
Latest reply on Oct 13, 2010 by Mr.Norm
Hi,

I need to measure S21 (magnitude & phase) of a frequency converter DUT, magnitude & phase tracking between number of up-converter channels.

1. Can it be done with the "Golden-Mixer Technique" ?
2. Witch options do I need for it for the PNA?
3. Must I do a Vector-Mixer Calibration or Scalar-Mixer-Calibration or regular Linear Calibration?

Thanks,
L.L.  

Outcomes