AnsweredAssumed Answered

OK to use High Temp Probe in sulfuric acid?

Question asked by inverse_era on Aug 6, 2008
Latest reply on Aug 8, 2008 by inverse_era
Can the 85070D high temperature dielectric probe withstand a liquid solution that is 50% sulfuric acid, 30% alcohol and 20% water?  I have attached the only documentation that I could find concerning my probe.  On page 2 it says “Hermetic glass-to-metal seal resists corrosive chemicals.”  I was wondering if it can handle a corrosive chemical like sulfuric acid at such a high concentration.  

Outcomes