AnsweredAssumed Answered

8510B VNA with 8514A?

Question asked by xpatriot on Jun 17, 2008
Latest reply on Jun 20, 2008 by RayH
Hi folks!

Can someone please tell me if an 8514A S-Parameter test set is compatible with the 8510B VNA? And is that spelled out somewhere in black and white?

Yeah, I'm on a fool's errand to bring this system back to life.

My RF source will be an 8350B + 83595A sweeper set. I have the 8510C preflight checkout sheet (though mine is a B model) . It was very helpful, but does not mention the 8514A at all. I'm trading in my 8516A 2.4mm test set for a 3.5mm one. I can get either the 8514A or the 8515A for it. I wish I could get an N-Type test set for the system, but oh, well.

Also, does anyone produce Verification-Kits with data on tape, or possibly correction data accessible through the IEEE? I saw one at Maury Microwave with a data tape, I think. Any suggestions on the best way to get traceable? Where to get the right kit? I heard that my VNA will be useless I can upload the verification data via tape. Why not through the HPIB interface?

Thanks for any help you can provide.

Outcomes