AnsweredAssumed Answered

HELP! chip inductor measurements L - SRF - DCR

Question asked by nono00 on Jul 4, 2008
Hi.
I need to measure the following features of an inductor (chip inductor):
1) L at 250MHz (aprox. 1.6nH)
2) SRF - SelfResonance Frequency (aprox. 12.5GHz)
3) DCR - DC Resistance (aprox. 0.03 ohms)

How can I do this with an network analyzer (some model)? Or with another instrument/s? Special probes? Test fixture?
Any comment is welcome.
Thanks

Ceramic Chip Inductor SMCC0603 (Wilco)
dimensions in mm: 1.8x1.12x1.02.  

Outcomes