AnsweredAssumed Answered

E4419B Power Meter & E8364B PNA GPIB control issue

Question asked by rickhart on Jun 20, 2006
Latest reply on Jun 21, 2006 by rickhart
Actually all I want to do here is use the E4419B power meter which is connected to the Performance Network Analyzer (needed for doing a source power calibration).

I need to do 2 things here:

1) Use the E4419B (connected to the PNA via a USB GPIB) for a source power calibration and.....

2) Use this same E4419B via an external controller to calibrate a couple Signal Generator's.

I can't connect the external controller's GPIB interface directly to the E4419B because it already has the PNA's USB GPIB interface connected to it.

Is there any other way to access the E4419B? through the PNA's LAN interface? through pass-through control?  

Outcomes