AnsweredAssumed Answered

N5230A Self Test

Question asked by RichardTripp on Oct 5, 2006
Latest reply on Oct 5, 2006 by jvall
While it is possible to get the status of the last self test via the SCPI "*TST?" command,  I was unable to find in the PNA Help (6.04) the means to force a self test.  Does such a command exist?

As for the results returned by the *TST? query, are they from a power on self test or does self test run continuously in the background?  

Outcomes