AnsweredAssumed Answered

Output Raw Data from ENA

Question asked by opticyclic on May 15, 2006
Latest reply on Jan 10, 2007 by opticyclic
I read that OUTPRAW1-4 to Output raw arrays 1-4 is not supported in the ENA.
Is the only way around this to display a1/b1, for example, then output the data?

This doesn't seem very elegant and causes a bit of confusion for the operator when the screen splits/changes from expected.  

Outcomes