AnsweredAssumed Answered

Multiple-channel measurements with a PNA

Question asked by Avery on Jul 28, 2006
Latest reply on Aug 4, 2006 by johanna_larmour
The Antenna Test selection guide 5968-6759 mentions using the 85331B/85332B PIN switches for multiple-channel measurements, but the only controller mentioned for these is the 85330A, which seems to be designed for use with the old 8530A microwave receiver.  How do I use the PIN switches with a PNA?  Will the 85330A work with the PNA?  Is there a better way of controlling the PIN switches from a PNA (i.e., with less latency than GPIB)?  How much software development would I have to perform to use the PIN switches with a PNA?
Thanks!  

Outcomes