AnsweredAssumed Answered

8510C w/8715B accuracies

Question asked by stat2883 on Jan 28, 2012
Latest reply on Oct 7, 2014 by crow
Hey,

I'm trying to create an uncertainty budget for our 8510 system, but I'm unable to find any stated accuracies for the system using an 85054B N-type cal kit as a calibration standard.  In the datasheet on the product webpage, it only gives values for the 3.5mm, 2.4mm, and some various other configurations.  Even those are just graphs and no real numbers that I'm seeing.  I need to determine uncertainties for all S-parameter measurements.

Is this information available out there?  I'm not having much luck.  If its something that I'm missing and already have the information I need, please point me in the right direction.

thanks,  

Outcomes