AnsweredAssumed Answered

Antenna measurement using PNA E8362B

Question asked by Hidayah on Apr 1, 2008
Latest reply on Apr 3, 2008 by Hidayah
Hi,

I have something to ask you regarding the antenna measurement. I have a transmitter antenna that will be connected to port 1 and a receiver antenna connected to port 2. My question is how to measure the the power that received by the receiver antenna using the power sweep measurement ? I want to use the VEE to read the measurement. So, I want to know what measurement should I set in it.

1. Is it I just need to set the input power for channel 1 and set S21 for measurement ?

2. Or is it I need to set the input power for channel 1 and measure the S21 at channel 2 ?

3. Or is it I need to set the input power for channel 1, and measure only the S11 for channel 2 ?

Thanks.  

Regards,
Dayah  

Outcomes