AnsweredAssumed Answered

PNA 8364B and Attenuator

Question asked by minzhe on Jan 29, 2007
Latest reply on Jan 30, 2007 by minzhe
I would like to put an attenuator in between the RF cable (cascade 132-424) and the PNA (8364B). I have checked the manual, and they only mentioned that the connector is 2.4mm. I'm wondering if this is a N-type connector and if i used a male/female n type attenuator, would it fit in this configuration?  

Outcomes