AnsweredAssumed Answered

Special Function 201 on 8645A

Question asked by malky on Apr 23, 2007
I am using the 8645A for frequency hopping in the following modes:
Int Repetitive and Fast Hop Bus Ext Dwell.
and I'm using an external source which is plugged in the FM or Phi-M ports.
Do I have any reason for enabling/disabling the 201 (buffered hop bus) special function? is this function relevant in this case?

thank you.  

Outcomes