AnsweredAssumed Answered

Is there any portable Network Analyzer.

Question asked by ehondaus on Dec 24, 2006
Latest reply on Jun 15, 2009 by dgun
Hello,

May I know if Agilent provide portable network analyzer?   Due to the NA is too bulky to be hand carry over the workplace, I am wondering if it is possible to compact all the thing to one DVD-ROM like USB 2.0 network analyzer.    

This concept is of course like a USB TV-Tuner.  The box would consists of connectors and power supply.  Special software is needed to load in order to simulate your pc as network analyzer.  I have used N5230 which powered by Windows XP and it is fantastic.  

ehondaus  

Outcomes