AnsweredAssumed Answered

firmware downgrade problem

Question asked by dain_miller on May 8, 2006
Latest reply on May 10, 2006 by odanzy
I upgraded the firmware on my PNA to version 6, then discovered that some non-agilent sofware didn't support it yet.  I "downgraded" back to version 4 successfully, but now the front panel keys don't work.  The usb mouse and keyboard work fine, and I can access the functions of the front panel through a pull-down menu, but this is not very convenient.  Has anyone else run into this problem or have an idea of how to fix it?  The PNA help suggested re-booting with no usb devices and then re-connecting them (this didn't help).  

Outcomes