AnsweredAssumed Answered

Move (drag) markers on the PNA N5230C screen

Question asked by colblimp on Apr 17, 2008
Latest reply on Apr 18, 2008 by colblimp
Hello.

My company has a N5230C PNA-L Network Analyzer, 2-ports, up to 40 GHz. It was bought in January 2007. When I use it, S-parameters are often behind the markers, but I can't drag them to see S-parameters and of course I need markers.

So, is there a way to move markers on the screen where they don't bother? (They are stuck in the upper right corner).

I can drag markers with ENAs and I'd like to do something equivalent with PNA. Is it possible? Thanks.

BR,

Colblimp  

Outcomes