AnsweredAssumed Answered

E5071C Calibration with probe-SMA

Question asked by RF_TJ on May 2, 2018

One port probe, one port SMA calibration using E5071C

 

I have the cal kits for SMA and probe, separately. But I to do a full two port calibration with port 1 probe and port2 SMA ?

If there is a way what will be the procedure. It seems like I can only use 1 cal file for the two ports.

 

Thank you.

Outcomes