AnsweredAssumed Answered

Exacting RLGC file

Question asked by aguntuk on Apr 6, 2018
Latest reply on Apr 6, 2018 by aguntuk

Hi,

I have created stripline/microstrip transmission line in ADS using Controlled impedance line designer (CILD). Now I want to extract the RLGC equivalent parameter file of that created transmission line. I know in the CILD option there is given RLGC parameter for single point. As RLGC parameetrs are frequency dependent I need to extract the RLGC per unit length for the created line so that i can use this for other lines in ADS or even in Virtuoso also. It would be nice if someone help me about this on how to do it. Is it possible from schematic or from the CILD tool? Here is an example of microstrip line that i created for just to show.

 

Microstrip Line

Outcomes