AnsweredAssumed Answered

How to Remote Program Test App

Question asked by rTranilla on Apr 5, 2018
Latest reply on Apr 30, 2018 by algoss

I'm working on a Python 2.7 script to automate the 'N5392B/N5392C Ethernet Test App' that's installed on our DSO90404A.

I'm able to connect with the DSO90404A and launch the test app using PyVISA.

I now want to connect to and control the test app using the .NET package for Python.  I used the example code from the Keysight DigitalTestApp Toolkit.  However, I encounter an exception when the script tries to create a Remote Obj

 

Here's a screenshot of my command-line sesson:

Exception when trying to create a RemoteObj

 

Any insight would be appreciated.

Kind Regards

Outcomes