Is anyone having trouble or success using the NI GPIB-USB-HS interface with VEE Pro 9.32 & Windows 10?
I keep getting Error 801 & 811 when everything worked fine in Windows 7. This is happening with three different PCs, all switched to Windows 10. The odd thing is that it HAS worked for a while on one Windows 10 PC, but now it has stopped working on that PC also. Have done Repair on VEE Pro 9.32, NI488.2, etc.: All with no success.
Make sure you're using the latest version of IO libraries.
https://www.keysight.com/en/pd-1985909/io-libraries-suite?cc=US&lc=eng
-Bill