I am trying to get Command Expert running to act as a starter for a Visual Studio 2017 (VB.NET Form) project. I can connect to and operate my 34461A Meter but I am struggling to connect a Rigol DP832A PSU. When I can't find the DP832A from Command Expert, it prompted me to run Connection Expert which found the DP832A immediately, the issue is that there is no SCPI command set - apparently there's a way to add a command set from the IVI Foundation's list (where the DP832A is a registered instrument. Any tips on how to do this would be appreciated.
Sorry for the delay. First you must install the IVI driver, of course. Then in Command Expert you click on New Instrument > Connect to a real instrument > Next > Select the instrument as found by Connection Expert > Next. It should now show both the SCPI and IVI driver choices. Select the IVI driver and then click on Next.