AnsweredAssumed Answered

Total Amplitude Visualization in Momentum Viewer

Question asked by HCH on Feb 26, 2018

The visualization tool of Momentum allowed the 3D visualization of the currents. Especially with the Addon "EM Circuit Excitation" ,that is a real advantage of ADS to connect schematic simulation with EM (FEM/Momentum).

But the EM current quantities are represented as steady state sinusoidal waves.

So far, I haven't understood why it should be more helpful to work with specific phase representations in practice. I'm personally interested in the amplitude in order to find the sources of losses.
In the FEM viewer, the representation of total amplitude is available. In Momentum not.
Has anyone an idea to solve that problem or bothered to create a workaround?

 

Thank you very much for help

Henry

Outcomes