Hi,
please clarify if the 2015 version of momentum support writing out a 20 port S parameter file (in touchstone format) from EM simulation and 20 port s parameter file reading through data component for schematic simulation.
following is the snapshot of the warning message i get:
also, is there a generic data component i can use for touchstone files with more than 10 ports? where can i find it?
To use SNP files with more than 10 ports, you can type in the symbol name (e.g. S20P) in the entry box directly:
The message that you showed above can be ignored, suffix s20p is fine.