On the basis that the 9000H series is still "supported" (and runs the latest 06.10 release of Infiniium) even though it's "discontinued" could we see BenchVue work with it? The 9000H cannot be that different to drive remotely than the 9000A which is supported by BenchVue.
Failing that, what options do I have other than the Web interface which is pretty poor?