Hi all,
My E4433B came with an ancient firmware version B.02.24, so I decided to upgrade it to the latest version (via the 2-step process, with B.03.20 as an intermediate version).
That didn't work out as planned, and the generator now throws up a number of errors:
ERROR: 617, Configuration Error
Installed option board not supported
RF OUPUT
REFERENCE BOARD
Illegal combination of installed option boards.
The "Installed board Information" shows:
RF OUTPUT E4400-60003 EOF CONFIG ERROR
REFERENCE BOARD E4400-60009 EOF CONFIG ERROR
(other boards are OK)
My guess is I'm dealing with an early version of the ESG "B", with 2 boards derived from the "A" version.
The information screen originally showed:
Model: ESG-D4000B
Options: 1E5,UN8,UND,UN5,H97
Serial Number: US3723xxxx
Firmware Revision: B.02.24 (ARB ver 1.2.05)
The question is: since it was working fine with firmware version B.02.24, how can I go back to that?
The oldest downloadable version is B.03.02, which doesn't work for my generator.
Thanks in advance and best regards,
Rick
Hi Rick,
Those configuration errors you see have nothing to do with the firmware revision. Either something went wrong with the firmware load, or you just got a coincidental failure such as dirty board connections or header corruption in the two boards. I've never seen headers become corrupted as a result of a firmware load. You options and board part numbers are fully compatible with that firmware revision. I suggest upgrading to the latest (B.03.86).
Regards,
Eric