Just wondering if anyone has integrated into their VEE programs, devices from www.Phidgets.com. To be more specific I recently got a temperature sensor device ( Phidget Temperature Sensor 4-Input, ID:1048_0B ) which has 4 inputs for K-type thermocouples and can communicate via a USB cable. I would like to integrate it into an existing P1dB VEE program that I have so that I can measure the temperature rise around a DUT at multiple points when the RF power is increased.
The Phidget Temperature Sensor works when I downloaded a driver for Windows and use a control panel GUI that Phidgets supplied. There is a lot examples on their website supporting software languages for C, C#, Labview, Visual Basic.NET, Python, Matlab as well as a few others. I tried loading the dll file and the .H file into VEE but it generated an error.
Without getting into the details right now. Has anyone tried using the 'Phidgets22' dll and supporting files with VEE?
I will also post on the Phidgets forum, but a brief search already made no reference to using VEE.
Thanks,
Declan
"I tried loading the dll file and the .H file into VEE but it generated an error."
That won't work as VEE does not read standard C header files, but instead has it's own version which is by default a ".def". The good news is that you have straight C examples so unless there are data structures involved creating a VEE header file and using the C DLL is very likley to work just fine.
Post the supplied header file to VRF (or here I suppose) and most likely someone will be able to translate it for you.
Or read VEE's docs (http://www.veeos.org/documents/E2120-90002.pdf will do - see the Compiled Function chapter) and you'll find that converting a C header into a VEE header is mostly taking into account the specific data types that the VEE interface can deal with.
Stan