Hello all,
I am working with the lab device N6705C to measure current for a certain amount of time remotely via LAN using SCPI and python scripts. I have looked through the lab device manual and have established a basic understanding of SCPI. I am still not sure about following things:
1: is there a command that triggers measurement on the device specific channel for the current? and then trigger to end the device current measurement?
2: what is the expected latency for the device via LAN. For example If I sent the command to start the current measurements after how much time it is acknowledged and the measurements actually starts?
Some quick guide lines will be helpful to get me going
Thanks alot.
Best,
Fahad