Hi,
I tried out various commands using Command Expert on a E36103A unit. However, I found out that SYSTem:RWLock,REMote does not work on this unit. Is this command really supported, or I need to update firmware?
PS: in SYSTem:VERSion? section, it is stated that the SCPI version should be 2005.0. However, I got 1999.0 when I ran the command
Thanks,
Hi neogeo4ever,
The firmware version is not the problem. I have tried out the remote and local mode commands that you mentioned using E36103A version 1999.0 and they work just fine. May I know what is the error returned after you have sent the command?