Trying to add a measurement into test flow, see no orange box to drag into the flow. It does show up in Workspace, but nothing to select.
Trying to add a measurement into test flow, see no orange box to drag into the flow. It does show up in Workspace, but nothing to select.
I am looking forward to the DAQ integration into test flow!
Will you send out this update automatically when it is available?
You will see a notification that new apps are available for download when you start BenchVue. In addition, the apps tab will have a flag on the DAQ icon that indicates a new version. Should be ready about June. Updates to the Scope and PS apps are to be released soon, and the DMM will also be getting a refresh, hopefully by the end of March. The Serial control app was just released. Lots of cool stuff happening.
Brian
The DAQ App today has only one function that can be used in Test Flow - state file load. We are adding much more capability in the next release of the DAQ App, and many other enhancements too. Watch for it this summer!
Brian Wood
BenchVue Support