I get "Oven Cold" error in E8267D and it's not disappearing even when the instrument is powered on for more than 2 hours! and when I clear the errors it comes up again!
The PSG is working fine but the error is still there ...
Is there any solution for this?
Hi Antonia,
It could be that the timebase oven has a failure, or possibly the rear panel interface board is at fault. Other than sending it in for repair, you might try reseating the ribbon cable that goes from the rear panel interface board to the CPU. That's part of the path for that indicator logic. Also see if the 10 Mhz output is on frequency. If the oven's bad that will be off freq.