Fieldfox N9916A with power sensor application installed and operating with U2021XA Peak and Average power sensor.
When a peak power reading is taken it remains on display, but how to reset this peak reading in order to take a fresh reading? Only way i have been able to do this is by disconnecting and reconnecting the USB connector to the Fieldfox.
Thank you, Andrew
What is the firmware revision of the N9916A? I thought we had fixed this issue. To check firmware,
[System] {Service Diagnostics} {System Information}
Read the third line, firmware release. Should be something like A.08.xx, or A.09.xx.
Also, do you have the new CPU (CPU2) or original CPU. Also, on same page, BIOS rev shows the CPU used in the analyzer.
Afsi Moaveni